(0)| 12/15/2023 8:37 AM | |
|
Joined: 8/3/2009 Last visit: 1/16/2026 Posts: 16644 Rating:
|
Hello Icoto create on the Runtime PC in the certificate manager a CA with your Runtime Station and then create a webserver certificate and install it. Then run the unified configuration again in the runtime pc and use the installed certificate. You can also use only IP Adress if there are problems with name resolution (then also the IP has to be used in the Certificates) then restart your system and RT Project. then if you connect to the server from the client in the Unified start screen there should be a new option do download the certificate for a secure https connection -> but you can also use an unsure connection for testing Check this FAQ for a little help: https://support.industry.siemens.com/cs/de/en/view/109806850 Hope that helps Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on