(0)| 6/12/2009 4:20 PM | |
|
Posts: 32 Rating:
|
We havePCS7 v6.1 projects with multiple redundant servers and several multi-clients. We have to integrate an existingthird party unit which is controlled by non-siemens PLC's and monitored with Factorylink scada. For Factorylink there is a migrationpackage to WinCC. According to the Siemens HMI Competence centre it is not possible to migrate to PCS7 directly. So we wonder if it is possible to replace the factorylink layerwith a 'standard WinCC' server and access it from the existing PCS7 multiclients. (Is it possible to port the clientpackage from the WinCC server into the PCS7 multiclient ???) (CoC was not able to answer this question (By the way....the migration to PCS7 for the complete unit is out of scope !) kind regards, Marcel |
Follow us on