(1)| 1/4/2024 7:23 AM | |
|
Joined: 9/9/2019 Last visit: 1/13/2026 Posts: 1 Rating:
|
Hello everyone, I have a question of testing Modbus ASCII driver with TIA V17, My structures are as below: Slave: When PLC connects to the controler via Modbus RTU, but when I use the Library FB of LModbus_AsciiMaster, then shows status: 8202 after retries. the communication parameters of controler are: here is the program and parameters: I have use my laptop to connect the controler via Modbus ASCII, is there something I need to revise? |
Last edited by: Jen_Moderator at: 01/04/2024 11:31:55Link optimized. |
|
Follow us on