(0)| 1/4/2024 2:20 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello HBCM; We might be quibbling about definitions here, but one thing has to be understood: in a client-server relationship there are no client-client application, there are no server-server exchanges.There are only client-server (active-passive) configurations. This is true in S7 comm setups, but lit applies to many computer-based exchanges such as OPC, WWW and email :https://en.wikipedia.org/wiki/Client%E2%80%93server_model https://www.matrikonopc.com/resources/opc-server.aspx Since a CP 343-1 Lean can only act as a server on PUT/GE applications, it must be connected to a S7 Comm client (for example a CP 341) and it will send and receive the data requested by the client. It will never initiate the requests. A CP 341, on the other hand, can be configured both as a server and as a client. As a client, it can request data from a server. As sancruz' screenshot illustrtes, on a second connection the CP 341 can act as a server to another client. In his drawing both CP 341s are setup both as client and as server, on two separate connections. But always the PUT/Get exchanges will happen between a client nd a server, never between 2 clients. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/04/2024 14:42:34 |
|
This contribution was helpful to
|
|
| 1/4/2024 4:04 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello HBCM; i am sure that anuone here interested in client-server applications (such as PUT GET exchanges) would be very interested in how you managed client-client configurations. if you can please post screenshots frm your configuration. You also add that the PUT GET instructions were programmed in both s7-1500 CPUs. In that casei would surmse that you are using a configuration that matches the following screenshot, with 2 parallel connections. PUT and GET can only be established with unilateral connections, from the client CPU (that includes PUT and GET instructions in its program) and a server. As discussed before, if both CPUs hare using PUT and Get, both can act as clients... but only with the server on the other CPU. I would recommend you look at the following link, especially at the Documentation links available for different cnfigurations. https://support.industry.siemens.com/cs/ca/en/view/82212115 That being said, since a client-client connection is not possible either in siemens programs or in any other client-srver applications, there is no point in discussing advantages of such configurations. hope this helps, Daniel Chartier |
Follow us on