(0)| 1/15/2024 7:12 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, If I understand this correctly, you would like to share/use input/output modules (from the CPU rack directly) with another CPU. What you would need is "shared device" and this is not possible for modules in the central rack of the cpu. If you would like to use shared device, the I/O modules must be connected via a distributed I/O system like ET200SP/ET200MP e.g. How, in STEP 7 (TIA Portal), do you configure access to a shared device and the function Module-internal Shared Input / Shared Output (MSI /MSO)?Otherwise I-Device and mapping of I/Os via user program.... regards sancruz |
Last edited by: sancruz at: 01/15/2024 07:16:38Feedback appreciated, please rate |
|
Follow us on