(0)| 1/16/2024 9:54 AM | |
|
Posts: 22 Rating:
|
Hello, I have the following device specifications: -CPU 1511F-1 PN V2.9 (6ES7 511-1FK02-0AB0) and CM 1542-5 V2.0 (6GK7 542-5DX00-0XE0) -IM 155-6 DP HF V4.2 (6ES7 155-6BU01-0CN0) -Tia Portal V17 I use the gsd file from this site: https://support.industry.siemens.com/cs/ao/en/view/73016883 and I still can't communicate IM155 module with CM152-5. I have the following error in the diagnostic buffer: IO device failure - Configuration fault (different configuration data). Profibus addresses are set appropriately. the communication cable is functional, it communicates with the inverter profibus card without any problems. Any help? |
Last edited by: Jen_Moderator at: 01/16/2024 12:07:04Link optimized. |
|
Follow us on