(0)| 7/13/2023 8:43 PM | |
|
Joined: 10/4/2022 Last visit: 7/20/2023 Posts: 7 Rating:
|
Hola, Me aparece el mismo error mencionado, pero no me establece conexión entre PROSAVE y HMI MTP1200 Unifield. En el Puerto X2 me aparece una IP 0.0.0.0 y la MAC en la esquina superior derecha. pero nose que IP poner en ProSave. Intento poner la IP del HMI pero no me resulta. Porfa si me pudiera ayudar con el tema, lo agradecería . Saludos. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/14/2023 06:44:53New subject after splitting |
|
| 7/14/2023 6:36 AM | |
|
Joined: 1/21/2013 Last visit: 1/16/2026 Posts: 4405 Rating:
|
Hi Leandro035,
Please write in English, as this is an English speaking forum.
Refer to the "Resetting an HMI device to factory settings via ProSave" section in the operating instructions. When configuring the IP address in ProSave, it is important to use a free address within the computer's subnet. To ensure that the address is free, it is recommended to use a direct connection from your PC to the Panel. Kind regards |
This contribution was helpful to
|
|
| 7/16/2023 6:08 PM | |
|
Joined: 1/21/2013 Last visit: 1/16/2026 Posts: 4405 Rating:
|
Hi Leandro035, Your PC may not have the correct settings for the PG/PC interface. Please follow the instructions in chapter "Setting the PG/PC interface". Kind regards |
Follow us on