(0)| 1/26/2024 9:06 AM | |
|
Joined: 10/30/2018 Last visit: 10/27/2025 Posts: 18 Rating:
|
Hello to all I used S7-1500 (512-1CK01-0AB0) in my project. I want to read values from another CPU (S7-1200) by OPC-UA. I wrote the program using library blocks 1- OPC UA Connect 2- OPC UA NamespaceGetIndexList 3- OPC UA NodeGetHandleList 4- OPC UA ReadList 5- OPC UA Connection GetStatus 6- OPC UA Disconnect When the program runs, the values are all read and live, but after a period of time between 15 minutes and 1 hour, the values are frozen. In this case, none of the blocks have Error and their Status value 16# is 00700000. What suggestions do you have to fix this problem? Kind regards M.Tavasoli ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/29/2024 08:25:59New subject after splitting |
|
Follow us on