(0)| 12/11/2023 7:28 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello; Problems can arise on optical networks from many sources: the fiber optic cable, the RS 485 Profibus connetor, the setup of the terminators, and other sources. Whenever we had to work out the kinks in our optical networks, we always started with the basic network troubleshooting steps, especialy examining the contents of te Diagnostic Buffer of the CPU. If the messages from the diagnostic buffer messages did not give a decent result, we would then follow the Torubleshooting guide from this manual: https://support.industry.siemens.com/cs/ca/en/view/109476821 I have attached the troubleshooting section of the manual as a separate attachment. Tell us if it provides adequate guidance. Hope this helps, Daniel Chartier AttachmentOptical link module- Troubleshooting.pdf (472 Downloads) |
This contribution was helpful to
|
|
| 12/13/2023 1:33 PM | |
|
Joined: 9/27/2017 Last visit: 1/13/2026 Posts: 22 Rating:
|
Hi Daniel, Thanks you so much for your answer. The thing is that device failure error is so short (around 50-100 ms) and sporadic, so it is hard to see the led behaviour when this happens. Yesterday we checked all connectors and we measured the signal quality (we got 4.3 V so the signal strength is so good). At this point the only thing we can test is reducing the power transmission using S5 dip switch, but I do not really think this is the problem as this architecture have been used many times without having this problem. If somebody has any idea about where could be the error I would be so grateful. Best regards |
| 2/7/2024 9:23 PM | |
|
Joined: 9/27/2017 Last visit: 1/13/2026 Posts: 22 Rating:
|
Hi all, Any other suggestions? we still have same problem and we did not find the origin.. Thanks! |
Follow us on