4/30/2024 7:32 AM | |
Joined: 10/5/2021 Last visit: 5/12/2024 Posts: 5 Rating: (0) |
Sorry, I missed that question. No, C is not spindle, it is the C axis like in this photo. When I move this handle the display changes a little. I can't move it more because I can't unlock the hidraulic. In the manual I have that is in german it shows how to move it but I guess it's not working because is not homed. It doesn't trow an error if I try to move it, just does not work. So I need help from someone with this machine maybe?!! |
Last edited by: crisiacuf at: 04/30/2024 07:32:53 |
|
5/1/2024 3:02 AM | |
Joined: 10/17/2007 Last visit: 5/12/2024 Posts: 3985 Rating: (342)
|
I do not want to augur with you --if you want to get help, you need follow my instruction and resposnse for my question-- see please answer!!!----you can run spindle --When running spindle, if C Axis display change or not after you confirmed I may help you to home C axis. and can you open the control cabinet to send picture and check how many drives you have? and you have German language operation manual --why you cannot use it. now almost no possible to wait for other people who have same kind of machine to help you
|
If you like my comments please |
|
5/10/2024 7:20 PM | |
Joined: 10/5/2021 Last visit: 5/12/2024 Posts: 5 Rating: (0) |
Thank for your patience! So when the spindle moves C axis display does not move. When I move the C axis handle the C axis display moves! I read and translated the geman manual and can't find anything about moving a manual C axis in it |
Follow us on