(0)| 5/18/2022 4:31 PM | |
|
Posts: 14 Rating:
|
Good morning I am trying to connect a Connect a ET200SP HA to a redundant 400 cpu. I have created the cpu's with a Profinet i/o system under each CPU ethernet onboard port . When i drag the IM155-6 PN HA with redundant interface (6DL1 155-6AU00-0PM0) to these Profinet i/o systems in Hw-config First the system ask me if I want to connect the redundant interface also on Profinet i/o system "B", and when I press "YES" software show me that "Not the same system family" Error #13.4016 . I have try to check on the card manual, but I haven't found a solution for my problem. Probably i have to set the I/O system differently, but I haven't understand how. Thanks
Attachmentimage.zip (724 Downloads) |
| 7/26/2023 11:04 AM | |
|
Joined: 8/1/2019 Last visit: 12/8/2025 Posts: 304 Rating:
|
I am struggling with the same issue here. Is there any solution? |
Follow us on