(1)| 3/6/2024 6:09 AM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, I am guessing you configure the server interface within TIA, right? If yes, the identifier is always "numeric", the standard server interface uses the identifier "string". As an alternative, you can configure the server interace with SIOME. There, also "string" like in standard interface is possible. There is an FAQ for S7-1200, but this should work for S7-1500 as well. How do you change the Node ID identifier type of the nodes in the S7-1200 OPC UA Server from "Numeric" to "String"?regards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on