(0)| 3/14/2024 1:54 AM | |
|
Joined: 2/11/2024 Last visit: 12/4/2025 Posts: 22 Rating:
|
Hi I use TIA Portal V18 and S7-PLCSIM Advanced 5.0 in Windows 11 OS. I am trying to simulate a S7-1500 CPU ( Article No.: 6ES7 511-1AK02-0AB0 FW: V2.5) with S7-PLCSIM Advanced 5.0 to test a simple MODBUS TCP/IP communication where S7-1500 will be client and my PC will be the MODBUS Server using relevant software. Until loading the program to the CPU instance in PLCSIM Advanced I have an established connection and I can ping the device through PLCSIM Virtual Ethernet Adapter. However, when I try to load the program for simulation, I get the following error in the Load Results: "Error downloading to device" Info window at the TIA Portal Inspector shows the following message: "Loading of HW configuration failed (0050 5 2 2458)." Would appreciate it if I can have some assistance in order to solve the problem. I have attached folder with pictures better reference. Thank you in advance. AttachmentPictures.zip (360 Downloads) |
| 3/14/2024 5:26 AM | |
|
Joined: 5/12/2006 Last visit: 1/13/2026 Posts: 22796 Rating:
|
and which messages are in the diagnosticbuffer? |
| 3/14/2024 8:21 PM | |
|
Joined: 2/11/2024 Last visit: 12/4/2025 Posts: 22 Rating:
|
Hi I checked the diagnostic buffer of the PLCSIM Advanced v5.0 device and I attach it along with some other pictures. If I understand correctly it seems the offline device and the device created in PLCSIM Advanced v5.0 are incompatible, however I am not able to understand why. Thank you for your assistance. AttachmentPictures 2.zip (326 Downloads) |
| 3/14/2024 9:18 PM | |
|
Joined: 2/11/2024 Last visit: 12/4/2025 Posts: 22 Rating:
|
Hi as well, I attach the Diagnostics buffer of the PLCSIM Advanced v5.0 Device as well as some other photos that might be helpful. Thank you. AttachmentPictures 2.zip (396 Downloads) |
Follow us on