(1)| 3/14/2024 12:30 PM | |
|
Joined: 11/2/2023 Last visit: 5/31/2024 Posts: 4 Rating:
|
The fundamental purpose of my project is the creation of a lemniscate, that is, the graphic representation of the infinity symbol in a continuous manner. To achieve this goal, I have developed an approach by subdividing the lemniscate into six circles, each with its corresponding arc, so that the shape of infinity can be accurately achieved. These circles are defined within a FC, called "trajectory", which, when invoked, executes the generation of the lemniscate. My approach to repeating these lemniscates on several occasions involves activating a signal at the end of the last circle, which, in turn, restarts the process from the beginning of the FC "path" (IMAGE 2). However, a problem arises at the moment of transition between one trajectory execution and the next, since a stop occurs that interrupts the continuity of the movement. So far it is the activation of a specific segment within the FC "path", which is executed when the variable "done_home" reaches a value of two (IMAGE 1). This segment, when activated, allows the repetition of the same trajectory cycle successively. It is important to note that the lemniscate begins and ends in the center, therefore, the stop is made at that point (when it passes for the second time, which is when it ends). The specific problem is the stop it makes when changing lemniscates, I want a loop of lemniscates without stops In the following link is the video of the simulation of the trajectory loop so that the stop can be better observed. AttachmentImagenes.pdf (440 Downloads) |
Last edited by: Irena.vami at: 03/14/2024 12:32:30Last edited by: Irena.vami at: 03/14/2024 12:34:20Last edited by: Irena.vami at: 03/14/2024 12:34:40Last edited by: Irena.vami at: 03/15/2024 08:51:12Last edited by: Irena.vami at: 03/15/2024 08:52:42Last edited by: Irena.vami at: 03/18/2024 08:11:17 |
|
Follow us on