(0)| 3/27/2024 6:29 AM | |
|
Posts: 3 Rating:
|
Dear Faseeh, I am also stuck with ccu3.4 but with a slightly different setup we have pcu 20 as an HMI My problem is that ccu is continuously showing RED on SF. Firstly i reset the whole system using NCk and PLC switches on ccu 3.4 which deletes the plc program and the bus error occur than i upload the plc program using STEP 7 now it still showing the red. Do i have to transfer NC files too using CARD/WINPCIN or this is the hardware fault to which i need to replace the ccu or could you provide me the winpcin software thanks in advance and lastly are you in Pakistan.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/27/2024 12:27:41New subject after splitting |
|
Follow us on