(0)| 4/1/2024 2:14 PM | |
|
Joined: 5/6/2022 Last visit: 1/15/2026 Posts: 589 Rating:
|
Hi Riyasa, In this case the remedy is somewhat the one you have followed, which you can see in the following FAQ: In some cases, I have seen that it has had to be installed and gone through all the SPs and updates to see which one it was installed with. The bad thing is what you mentioned, that since it is a discontinued version, the files cannot be found on the SIOS website. You can still configure them by talking to a sales representative or Support. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
| 4/2/2024 4:59 AM | |
|
Joined: 3/30/2020 Last visit: 1/19/2026 Posts: 5660 Rating:
|
There is no difference between Step7 V13 SP1 and Step7 V13 SP2 when it comes to CPU download / upload. But there is a big difference with Step7 V13 (without service pack). This is your problem. Review and execute the following procedure: |
|
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
|
|
Follow us on