(0)| 4/10/2024 8:01 PM | |
|
Joined: 12/9/2022 Last visit: 9/24/2025 Posts: 8 Rating:
|
At the same time, we write a serial number in the header area of several DBs with the same structure using the "S_Move" command. Later in the process, these DBs are provided with measured values and then retrieved and saved by an MES system. We have the following phenomenon very sporadically (approx. once a month). The first time the DB is retrieved, the wrong serial number (the previous serial number) is read out; the second time the same DB is retrieved, the correct serial number is read out even though the serial number has not been rewritten. Using a little logic, we compared the serial numbers of the different DBs with the same header and recorded a trace if there was a discrepancy. The trace was recorded, which is why I suspect that the DBs are written differently, but I cannot currently explain why. It is also strange that the serial number is correct again on the second readout of each DB. In addition, there are 15 minutes between the first readout of the DB "Component busbar" and the last DB "Measure" readout, but we have the same phenomenon. The first readout reads out the previous serial number and the second reads out the correct one. I hope I have described the problem sufficiently and clearly. Please do not hesitate to contact me if you have any further questions. Yours sincerely Yannik Koudelka AttachmentTIA_v15.1.0.8_Fehler ELAM-Kommunikation.pdf (279 Downloads) |
Last edited by: AutoGen_8746056 at: 04/10/2024 20:16:00Last edited by: Jen_Moderator at: 04/11/2024 08:02:57Text formatting optimized. |
|
Follow us on