(0)| 4/21/2024 11:49 AM | |
|
Joined: 7/16/2019 Last visit: 1/6/2026 Posts: 17 Rating:
|
Good day, We need to install a new SMI20 to a motor connected to a SINUMERIK 828D controller. Problem description: After connecting the SMI20 and power ON the machine, we had: 1- Alarms: 231150, 231806, 207565, 201840; all are related the encoder, the temperature sensor of the motor was read correctly by the controller. 2- The topology displayed the message for the SMI module " Wrong component plugged into target: SMI20_16 (T-26119428) ACTUAL SMI20_16 (T-RD6212427). " The new SMI20 is T-RD6212427. Troubleshooting: 1- I tried to restore the drive archive file (.ard), which was made before the SMI20 problem. But I get the same alarms. 2- I tried to download the SMI data with the parameters 4690/4691 as below: a- Set 4690 = 16 (SMI component number) b- Set 4691 = 2 (Download SMI data) I get the error below: 4691 = 11 (SMI data backup for the component selected not found). Motor: 1PH8107-1DG02-0DA1 Serial number: YFM2622299301001 SMI20: 6SL3055-0AA00-5MA3 / 5193004021. Please see the attachment. Could you provide a solution to install the SMI20 module? Kind regards AttachmentSMI20 _ Installation.zip (585 Downloads) |
|
kind regards |
|
| 4/23/2024 6:04 AM | |
|
Joined: 1/24/2021 Last visit: 12/27/2024 Posts: 196 Rating:
|
To be able to restore backup data to SMI module You should make backup before. So if have not done this before you have no data for restoring. Try to connect old SMI module and make backup of module data and then restore it on new one. Also u can contact local Siemens they will help you. And by the way this is asynchronous motor (spindle of lathe) and you have position encoder on it, so it seems you can change topology to work only with position encoder. I attached doc that provides information about backup/restore procedure on SMI modules. AttachmentSMI data back-up.pdf (710 Downloads) |
|
People are divided into those who do Backup and those who will do it. |
|
This contribution was helpful to
|
|
Follow us on