4/29/2022 12:20 AM | |
Joined: 4/29/2022 Last visit: 5/28/2024 Posts: 1 Rating: (0) |
Can not connect to the DXR. I get a error code stating “Unable to initiate BACnet stack. Verify the IP address are valid and there is no IP address/UDP port conflict with another application that is now running” I do not have anything going in the back background, I turned off Zscaler and verified my IVP4 in the Ethernet properties is in Auto find for the IP address. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/29/2022 12:39:04New subject after splitting |
|
Follow us on