(0)| 6/4/2024 6:49 AM | |
|
Joined: 6/4/2024 Last visit: 6/5/2024 Posts: 3 Rating:
|
-Operating System: Windows 10 - TIA Version : 17 - Hardware Modules numbers : 6ES7512 1DK01 0AB0 (ET 200 SP) 6ES7135-6HD00-0BA1 (AQ 4xU/I ST) I have a mass flow controller that is normally closed. For it to open and control the flow rate I need to provide a signal between 0 and 5 volt. For that I have an ET 200SP with an an AQ 4xU/I ST. I have not that much experience with TIA Portal (near none). I have been watching some videos and so I copied what they did for my case. Image of my configuration: [snip] The issue I am having. It is actually performing the calculation, but the controller is not actually opening. Furthermore, I disconnected the wires of the controller and connected my multimeter and what I saw was, that the voltage went up to around 2V and then dropped quickly again to 0... So I am not sure if there should be something done, so that the voltage keeps up and does not decay. I Tested with an external power supply to provide the 0-5V and the connection works fine (So the wires are not the problem). Also I got the TIA Portal to show me the current value for the actual value of the mass flow measured by the controller... So yeah, the issue is just to get the output module to provide a constant analog signal...I was checking the datasheet as well as my TIA Portal configuration of it and it is already set to 0-10V. Do you have some idea what could the issue be? |
Last edited by: Jen_Moderator at: 06/04/2024 09:06:12Link removed and file attached. |
|
Follow us on