11/2/2020 10:49 AM | |
Joined: 10/3/2010 Last visit: 11/18/2024 Posts: 1563 Rating: (192) |
With VBS you can read the actual OutputValue and also the complete list of assignments:
When you have this, you can write code to filter the actual assignment text based on the actual output valuie. As far as I can remember, directly reading the current assignment text is not possible. Some not documented and not supported VBS code/methods might exist, for example:
The above code works in runtime but is not documented and also is lost after stopping runtime. |
Last edited by: SteBo at: 11/02/2020 11:03:49Last edited by: SteBo at: 11/02/2020 11:08:30B r g d s , |
|
This contribution was helpful to3 thankful Users |
7/6/2024 3:51 PM | |
Joined: 10/24/2016 Last visit: 11/13/2024 Posts: 2 Rating: (0) |
solved my problem,many thanks |
Follow us on