7/29/2024 7:22 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, the PROFIBUS master must not be configured within the same project as the slave. But the slave has to be added and configured into the master project. Basically you can use this FAQ as a reference. The FAQ is obviously not an S7-1200 but the principle is the same with any PROFIBUS master <-> i-slave communication. How to you connect the communication module CM 1542-5 or the communications processor CP 1542-5 as I slave in STEP 7 V5.x to an S7-300/S7-400 CPU?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
2 thankful Users |
Follow us on