(0)| 3/16/2024 3:42 PM | |
|
Joined: 11/26/2021 Last visit: 1/9/2026 Posts: 12 Rating:
|
Why if i only want to send a Real form my UDT to a New Faceplate popup.? I have made a OnScreenKeybord Faseplate there takes a Real as a Paremeter. And from my Settings Part of my first popup i want to set 5 different Reals with the OnScreenKeyboard.? Is that possible? Only to send Part of and UDT (One Real) to a new chiled Faseplate. I would like to use the OnScreenKeyboard Faceplate in many orher Faceplates. And if i have to Parse the Compleate UDT i will have to make a OnScreenKeyboard for eatch paremeter i will like to change. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/18/2024 12:27:17New subject after splitting |
|
| 8/2/2024 8:55 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello AutoGen_9469921 Here are some information for using OSK: https://support.industry.siemens.com/cs/de/en/view/109825756 And additionaly it works also if you activare the tablet mode of Windows. Then the OSK opens also automatically without using kiosk mode Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on