8/2/2024 9:19 AM | |
Joined: 6/13/2019 Last visit: 10/31/2024 Posts: 2 Rating: (1) |
The "new" TIA Admin is actually trash. The UI is clunky, there is no clear indication of install progress, installs happen silently (and fail silently) & most times I have to install any updates manually. This morning, I opened TIA Admin & it updated itself - no indication of anything, the icon just disappeared in the task bar when hovering over it after a while. Rebooted & "localhost refused to connect." Downloaded the latest version from support - install - reboot - wait for services to start - double click TIA Admin icon - same issue. The worst update client I've ever used hands down. While the older TIA admin also had it's issues - at least I could use it. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/05/2024 08:15:33New subject after splitting |
|
Follow us on