8/2/2024 4:05 PM | |
Joined: 3/23/2020 Last visit: 9/19/2024 Posts: 10 Rating: (0) |
Hello,
Here is the example workflow: 1. These are the parameters I am trying to change: 2. I have already tried using Openness Explorer 3. But unfortunately I could not find a proper service that would provide the parameters in any way ...
I have even tried to do it through CAX export/import where I have thought that the CAX workflow would work in this situation but unfortunately it seems that it does not work. I have already tried to search these solutions here on the forum. - Attributes of a GSD device in Openness - 293146 - Industry Support Siemens but unfortunately these topics were not properly answered. Any help would be appreciated! Kind regards vformanek |
Last edited by: vformanek at: 08/03/2024 10:32:03Last edited by: vformanek at: 08/03/2024 10:33:17Last edited by: vformanek at: 08/03/2024 10:34:54Last edited by: vformanek at: 08/05/2024 06:35:06 |
|
8/6/2024 7:37 AM | |
Joined: 3/23/2020 Last visit: 9/19/2024 Posts: 10 Rating: (0) |
I have been investigating this issue for a while now. And yes comparing each property/attribute name is not that hard. But as can be seen on my post above, the Openness Explorer cant see the attributes that represent the parameters... What is weird is that I have even tried to import a safety device GSD and there only a few safety attributes are unlocked. My investigation has gone to that it could be an issue with versions since I am still using TIA V17. I will try with the newest TIA V19 since there are new features like:
- source here: Sales and Delivery release of TIA Portal V19 - ID: 109821307 - Industry Support Siemens
|
Follow us on