1/15/2024 12:54 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello Savage123 Webnavigator in Webbrowser is only released with Internet Explorer, not with other Browsers. there is also an Option with compatibility mode for Edge but also there has to be installed the IE: https://support.industry.siemens.com/cs/de/en/view/109792981 If IE is not installed or cannot be used, use the WinCCViewerRT.exe Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
8/1/2024 2:46 PM | |
Joined: 3/15/2024 Last visit: 2/25/2025 Posts: 1 Rating:
|
Hello, may I ask you what windows version was used ? windows 10 or windows 7 ? thanks |
8/7/2024 12:19 PM | |
Joined: 8/3/2009 Last visit: 9/15/2025 Posts: 16409 Rating:
|
Hello Aleksei WinCC V8 is not released with Win7! check the compatibility tool for all possible and released combinations of WinCC versions to OS versions: https://support.industry.siemens.com/cs/ww/en/view/64847781 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on