(0)| 10/6/2010 10:40 PM | |
|
Posts: 1742 Rating:
|
Hello, for FW 2.3 update, there is an entry like this one in the support pages http://support.automation.siemens.com/WW/view/en/42122470 Here an extract of that link: With update V2.3, the CP 343-1 Lean (6GK7343-1CX10-0XE0) is functionally compatible with the predecessor version. It can therefore be configured with the same STEP 7/NCM version (configured as in the past as a CP 343-1 Lean (CX10) with V1.0/V2.0/V2.1/V2.2). It is not necessary to upgrade STEP 7 or NCM when using the compatible functions. In other words, new compatible versions do not necessary appear in the HWCatalog. Only new versions with new features will have an explicit entry. |
Last edited by: jklm at: 10/6/2010 10:44 PM |
|
This contribution was helpful to
|
|
Follow us on