(0)| 12/2/2021 8:53 PM | |
|
Posts: 1 Rating:
|
Ricki i have very very same problem. With RW5.16 and CP1616 do u even solved This problem? |
| 2/15/2023 10:51 AM | |
|
Joined: 3/6/2018 Last visit: 6/3/2025 Posts: 1 Rating:
|
Hello, I Have the same problem, did you solve this? It would help me a lot! |
| 9/19/2024 2:07 PM | |
|
Joined: 8/14/2024 Last visit: 9/19/2024 Posts: 1 Rating:
|
Ok, let's go step by step I had the same or very similar problem trying to install an ET200SP 2024 on an ABB 2012 robot. To solve my problem, I had to create a project in TIA Portal with the hardware structure and then create an xdb to download to the robot. The problem I had was that the version of TIA Portal that I use is v14. This version does not have the ET200SP compatible with my physical hardware. So I called a friend who had TIA Portal v20. This version was not compatible with the robot. In a third project, I managed to use TIA Portal v17, which was compatible with the board and the ET200. I will share the project here. Have a good time!
AttachmentB.remuska.zip (531 Downloads) |
Follow us on