(0)| 9/25/2024 10:31 AM | |
|
Joined: 7/11/2022 Last visit: 11/11/2025 Posts: 59 Rating:
|
Hello, I use a single user project, I have a license for 1 web navigator. Following the tutorial in LINK, I was able to enable the WebNavigator on the "server" computer, and I properly load it both in WinCCViewerRT and in the web browser. The server computer has WinCC V5 and Windows 11 pro 23H2 installed, while the "client" computer on which I cannot load WebNavigator uses both Windows 11 education and win 11 home. A picture of the loading screen is attached. When I set the view in microsoft edge, without IE compatibility, the homepage opens with a download hub ( normal behaviour). Any solutions? |
Follow us on