(0)| 9/21/2024 12:59 PM | |
|
Joined: 10/19/2020 Last visit: 12/4/2025 Posts: 5 Rating:
|
hi all, i am trying to make one cpu 1500 to communicate with a simotion D425-2 as io device, in the same project. I attach some imgs to explain the situation. the issue is: network seems fine but the two devices cannot see their respective configured IOs. The only signal that there is a problem is that on the PLC i get "io-device problem: not supported configuration" but i do not have any clou on the why!! sorry for my english, is not my mother language. thanks to anyone who will help me! Attachmentimg.zip (509 Downloads) |
| 9/27/2024 8:54 AM | |
|
Joined: 8/3/2009 Last visit: 1/9/2026 Posts: 16629 Rating:
|
Hello ploppolissimo check out this Example: https://support.industry.siemens.com/cs/ww/en/view/109478798 There is also a chapter with Simotion as I-Device Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on