9/16/2024 5:04 PM | |
Joined: 7/11/2008 Last visit: 10/7/2024 Posts: 45 Rating: (1) |
I've installed HMI Panel Image Updater, followed to the letter this readme for that, and I cannot login. I have no error, no message, login button after pressed is gray for 3 secs and then get back to blue and can be pressed again. I've tried username I use for SIOS login, I've tried email registered to my account, nothing. I've tested these credentials just to check if I'm crazy with ALM and it is logged in. Why do I need this? I have TP700, with image V15.0.0.0. Project is made in TIA Portal V19, HMI device in project is V17.0.0.0 and I cannot select newer i.e. V17.0.0.8, only older, V16.0.0.0. I have installed all versions from TIA Portal V13 SP1 Update 9, latest V14, V15.1, V16, V17, V18 and V19 (latest meaning latest update). I've updated image in TP700 to V17.0.0.8 using ProSave, that was not possible from TIA Portal V19 it cannot find files, compiler says. I cannot change device in TIA Portal, to select HMI TP700 with V17.0.0.8, just V17.0.0.0. therefore, i cannot download project. do not know what to do anymore. Btw, I have installed panel images V17 update 8. any help, this is frustrating. thanx ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 09/17/2024 09:19:29New subject after splitting |
|
9/17/2024 1:50 PM | |
Joined: 7/11/2008 Last visit: 10/7/2024 Posts: 45 Rating: (1) |
this is the way I solved it: so, I've downloaded image V17.0.0.0 from i.e. copied folder in zip file V17 to the path above, although it is not necessary, could have unzip it anywhere. Then I point ProSave to this folder (images\CP_7_9), and did update firmware. Now, TP700 has firmware V17.0.0.0, which is what is available in TIA Portal V19 project and now I can download my application. spent two days to solve this thing. I got the message: buy Unified panels! hope this is helpful to someone. regards |
Last edited by: Moderator_Lan at: 09/17/2024 14:10:15link optimized |
|
This contribution was helpful to1 thankful Users |
9/20/2024 12:17 PM | |
Joined: 8/3/2009 Last visit: 10/15/2024 Posts: 13931 Rating: (1757)
|
Hello the same as here: Bye Murof |
If this Information really helps, you could use the Rate function |
|
10/1/2024 1:15 PM | |
Joined: 10/1/2024 Last visit: 10/1/2024 Posts: 2 Rating: (0) |
If the PIU installer does not work for you, please proceed as follows to install the V17 Upd8 images: Under the link below, item "1.2 Offline Installation Panel Images V17/V16 recommended for upgrade", you will find the panel images that can be installed without setup. These are described as TIA V16 and V17, but you can use those of V17 for TIA V19. You must unzip the zip file and copy it to the corresponding TIA 19 folder. The path for the correct folder can be found in the readme file for the panel images. Attachment109825750_Readme_Offline_Installation_Panel_Images_en.pdf (165 Downloads) |
Follow us on