(0)| 10/2/2024 10:57 AM | |
|
Joined: 5/6/2022 Last visit: 1/22/2026 Posts: 589 Rating:
|
Hi AutoGen_8232177, In this case, yes, you will be able to work normally since the higher licenses are backward compatible with previous versions. With this license you will be able to work on everything in engineering. The only problem you may have is that, as you say, problems may arise with the tags configured in the project since you exceed those allowed by your license and you must increase the tags. In any case, when you migrate the project it will tell you that you need it. I recommend that you perform the test to update the project. Best regards! |
|
If this Information really helps, you could use the Rate function |
|
| 10/3/2024 11:56 AM | |
|
Joined: 5/6/2022 Last visit: 1/22/2026 Posts: 589 Rating:
|
Hi AutoGen_8232177, In the case of WinCC Professional, you must have the following: - WinCC Professional to be able to work as an engineer (which you already know from what we have discussed) - WinCC RT Professional, which is used both to perform simulations and to load projects to work on. Without this component you will not be able to perform Professionals simulations. To acquire it, an additional license is needed as you can see in the following link: "SIMATIC WinCC V17 Runtime (TIA Portal)" I hope I have clarified your doubt.
|
|
If this Information really helps, you could use the Rate function |
|
Follow us on