(0)| 10/15/2024 5:15 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, I assume you mean the text for the inputs In01-In16. I suggest you use the "OS additional text" for In01 to In16. The total amount of characters for this attribute is 24. You can then assign a logic result for example: Yes/No for Text1 and Text0. See attachment. PS: Do not fill in the OS additional text for In01.Value, but assign it for In01, otherwise the text is not shown. The character limit is a system attribute and you can not increase it. |
Last edited by: Oreca at: 10/15/2024 05:17:27If I could help you, you can use the RATE button. Thank you. |
|
Follow us on