(0)| 10/15/2024 7:46 AM | |
|
Joined: 8/3/2009 Last visit: 1/15/2026 Posts: 16635 Rating:
|
Hello AutoGen_2969405 do you mean the WinCC RT Advanced as SCADA (its not a real SCADA System but anyway...)? The ethernet ports on the TP700 are only one ethernet card. It s kind of a switch. So you can do your topology as whon in the screenshot as a line topology, this works but you have to use IP addresses in the same subnet. To communicate with the Advanced RT with the S71200 check out this FAQ: https://support.industry.siemens.com/cs/de/en/view/89852595 And check also the communication ressources of the PLC: https://support.industry.siemens.com/cs/de/en/view/109479986 But generally it works to connect multible HMIs on the PLC Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on