(0)| 10/15/2024 12:07 PM | |
|
Joined: 2/27/2024 Last visit: 1/15/2026 Posts: 26 Rating:
|
Hi Daniel possible im struggling with similar problems Project is written in TIA v18 DP/PA link is as follow: IM153-2 (153-2BA02-0XB0) FDC157 (157-0AC85-0XA0) I tried using the GSD tool, but im unclear whether i should add the FDC gsd file to the compilation directory....but i tried both with and without the fdc gsd file.. main issue is the IM153-2 is not visable on the hardward config, althou i can detect it on the DP network from the CM (cm1542-5) any advice is welcome at this stage dchartier
------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/15/2024 12:16:28New subject after splitting |
|
Follow us on