(0)| 6/27/2009 3:46 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello, First of all, you have to print a report after finishing a batch. So you should have in this report some variables. In WinCC flex. go to reports. create a new report. It will opens a sheet. Now begin to design your batch report and you have to link it with the tags of the variables to be displayed in the report. like qty of material used, time of starting the batch, temperature of water in tank 1 at starting of the batch,...etc. Then create a tag. it may be int, bit,...DINT. At certain value of this tag the report should be printed. So you have to have a printer connected to the panel. To do so, please read the following FAQ: How can you do a report logging, a hard copy or report printing on a printer with Windows-based panel via HyperTerminal? Regards, |
|
Ayman Elotaify |
|
| 6/28/2009 8:32 AM | |
|
Joined: 9/18/2006 Last visit: 12/8/2025 Posts: 596 Rating:
|
Hi.
AttachmentWorking with reports.pdf (506 Downloads) |
This contribution was helpful to
|
|
| 6/30/2009 2:39 AM | |
|
Posts: 241 Rating:
|
Thanks Anyman. |
Follow us on