(0)| 10/18/2024 6:39 AM | |
|
Joined: 3/12/2024 Last visit: 12/19/2025 Posts: 230 Rating:
|
Hey machado_john, it appears you're experiencing a specific issue with the SIMATIC IOT2050 FS 08 and 128 GB Samsung Evo Select micro SD cards. I am not aware of any such case. Maybe this are potential solutions: Firmware Compatibility: The FS 08 version might have a different firmware that's not fully compatible with certain high-capacity SD cards. Check if there's a firmware update available for your FS 08 device that might address this issue. You can find updates on our Download Page. Boot Order Configuration: Verify the boot order settings in the FS 08 device. You can check the current boot order by connecting via serial console and typing
If necessary, adjust the boot order using
SD Card Partition Scheme: Ensure the SD card has the correct partition scheme for booting. Use a tool like Rufus to create a proper bootable SD card image. Hardware Compatibility: There might be a hardware-level incompatibility between the FS 08 and this specific SD card model. Try using a different brand or model of 128 GB SD card to see if the issue persists. We originally made the following recommendation on Micro SD Cards:
We have not yet tested additional cards. BR |
Follow us on