(0)| 10/21/2024 8:14 AM | |
|
Joined: 7/19/2022 Last visit: 1/14/2026 Posts: 436 Rating:
|
Hello AutoGen_3333661, Does it mention a specific address in the diagnostic buffer? Sometimes the process images of the CPUs come by default at the minimum. For example, in the CPU 414-3, by default the input/output process image is configured at 256 bytes and can be configured up to 8 kbytes. If you are trying to access an address higher than 256 and you have not increased the process image from the CPU Properties > Cycle, you will not be able to access that address. It is not recommended to increase the process image to the maximum if you are not going to use so many addresses, since it can affect the cycle time. |
|
If this Information really helps, you could use the Rate function |
|
Follow us on