10/21/2024 10:15 PM | |
Joined: 2/17/2020 Last visit: 2/25/2025 Posts: 29 Rating:
|
Hey guys, I'm in need of help. I'm making a change to a plc but I don't have a backup. This is a 1200 cpu 1214C firmware version V4.2.0. And when I upload the configuration they bring all the blocks in the correct way, but they do not bring the hardware configuration with their respective network nodes. On the forum I found 0_Einstein's answer talking about the version, and that it would not be possible to upload it. Is there anything that can be done in this case?? LINK: 0_Einstein's answer https://support.industry.siemens.com/forum/br/en/posts/(s7-1200)-tia-portal-cannot-upload-the-full-hardware-configuration/287859 |
Last edited by: Moderator_Lan at: 10/22/2024 07:43:41Text formatting optimized |
|
10/22/2024 5:21 AM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
how you perform the upload exactly? |
10/22/2024 6:18 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi, use method "N" as shown in this FAQ, but make also sure the preconditions shown in the FAQ for the TIA versions are met. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?Otherwise, more details about the issue. Screenshots, error messages, description how the upload is performed in detail e.g. regards sancruz |
Feedback appreciated, please rate |
|
Follow us on