(0)| 10/22/2024 1:50 PM | |
|
Joined: 11/29/2011 Last visit: 2/4/2025 Posts: 1362 Rating:
|
Hi, I am implementing a modbus interface to a few heat meters. I am using the example: Master-Slave Communication via a CM PtP using the Modbus RTU Protocol The way my slave specifies the variables confusing me. I am using the "Master_Modbus" block to request data from the slave. I specify the number of slaves on the bus using the No_Slaves parameter Then I go to the Comm_Data DB and set up what information I read out of the slave. But how to set it up to read all of the data out of the slave(the description is bellow). Modbus Slave Description: Modbus RTU Modbus/KMP TCP/IP - molline.de What I am really unsure is can instanciate the "Data_for_Master" udt to read out all that information at once? |
|
- What you read here, please check with manuals and your requirements. |
|
Follow us on