(0)| 10/16/2024 12:22 PM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi,
open user communication is performed asynchronous! So depending on the cylce time of your CPU and amount of data to be send/received, the communication process (each call) may take several cpu cycles! Difference between synchronous and asynchronous instructionsTRCV: Receive data via communication connectionNote Because "TRCV" is executed asynchronously, the data in the receive area is only consistent when the NDR parameter is set to the value "1". regards sancruz |
|
Feedback appreciated, please rate |
|
Follow us on