(0)| 10/18/2024 9:45 AM | |
|
Joined: 2/27/2024 Last visit: 1/20/2026 Posts: 26 Rating:
|
Hi Im having the same error Interplc connection setup using static method in TIAv18 Connection type: Configured static S7 connection protocol: s7 protocol via ISO-on-TCP Online status: disconnected Connection>> Properties>> Adress details (partner, 03) for active connection but communicating PLC is step7 project, Connection status in NetPro: Setup Green ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/18/2024 09:54:37New subject after splitting |
|
Follow us on