10/28/2024 8:01 PM | |
Joined: 5/29/2019 Last visit: 7/10/2025 Posts: 8 Rating:
|
Hello i have S7-300 CPU 315 2 DP which is connected to CU320 2DP (SINAMICS S120) via PROFIBUS in a existing installation i have downloaded the GSD files from the link : https://support.industry.siemens.com/cs/ww/en/view/49216293 i have installed the GSD file for the relevent version of my CU320 with sucess, but my problem i can't find the CU320 in HW catalog ? i did not understand why ? please help |
Last edited by: Moderator_Lan at: 10/29/2024 08:21:52link optimized |
|
10/29/2024 10:19 AM | |
Joined: 7/19/2022 Last visit: 9/8/2025 Posts: 436 Rating:
|
Hello AutoGen_7012571, In GSD, devices with generic references appear (6SL3040-1xA00-0xxx or 6SL3040-xxA00-0xxx), therefore you must search for it from Device & networks > HW Catalog > Other field devices > PROFIBUS DP > Drives > SIEMENS AG > SINAMICS and use the generic reference of the corresponding firmware. |
If this Information really helps, you could use the Rate function |
|
10/29/2024 12:57 PM | |
Joined: 5/29/2019 Last visit: 7/10/2025 Posts: 8 Rating:
|
Step 7 manager V5.6 |
Follow us on