(0)| 10/28/2024 1:52 PM | |
|
Joined: 9/21/2024 Last visit: 5/14/2025 Posts: 8 Rating:
|
Hi dear friends I have a problem with the Siemens Basic Basic Panel KTP1200 ) via Tia portal 17 First, I don't have any access to the panel settings , and I want to reset the panel, but when I want to connect to the panel I see the typing interface on the ISO if the panel is not on the PN / IP. It was, and I do whatever I change this setting, I won't succeed (except once when it changed and I lost it !!) What can I do? When I want to connect to the panel via the Tia portal, the interface type is on the ISO and the laptop does not connect to the panel, and what I tried to change it to PN / IE was not replaced (except once as a chance That I forgot about how it was) Peaaaaaaaaaaaaase help me soon !!!! ------------------------------------------------------------------------------------------ |
Last edited by: navid_neshat56 at: 10/28/2024 13:57:42Last edited by: Moderator_Lan at: 10/28/2024 16:19:43New subject after splitting |
|
| 10/28/2024 4:51 PM | |
|
Joined: 2/17/2020 Last visit: 1/19/2026 Posts: 1251 Rating:
|
Hi, As you cannot communicate your PC with the Basic Panel, is it possible to perform the reset via USB in your case? Please see: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels |
|
A rating will be well appreciated. |
|
Follow us on