(0)| 11/17/2023 7:41 AM | |
|
Posts: 2 Rating:
|
Hey y'all , hope you all doing well. I have a little problem, please. In fact, I have a DSE7320 which is a generator controller and I want to access its datas on my plc. I've followed the siemens turorial so that I'm using a ET200SP, and a CM PtP as the dse7320 supports rs485. I've connected the wires ( Transfer, receive and ground ) the right way, and I think I did the right way the config of the 02 blocks that I used (Modbus_comm_load and Modbus_master), But unfortunately, nothing. The fun fact is, there is no error message, the status is 7000 which means no operations is processing I think , but sometimes the ''BUSY'' of my modbus_master block is switches to 1. I will put the snapshots in a ppt file just below because I didn't manage to send many files in a row. Attachmentsystemsnapshots.pptx (1053 Downloads) |
| 11/21/2023 7:24 AM | |
|
Posts: 2 Rating:
|
Hey, Thanks for the feedback. I don't know if it matters but it's a DSE 7320 MKII, and on the datasheet, there is MODBUS RTU (Either with RS232C or RS485). Find attached please, the 2 pages data sheet. Thanks, AttachmentDSE7310-DSE7320Data-Sheet-(USA).pdf (1265 Downloads) |
| 11/7/2024 3:55 PM | |
|
Joined: 5/28/2015 Last visit: 7/30/2025 Posts: 24 Rating:
|
Hi
Modbus Master Modbus address 10 Mode 0 Data address 41025 Data LEN 66 Modbus load ---> Mode 4 (into the DB) Baud 115200 |
Follow us on