(0)| 11/5/2024 2:56 PM | |
|
Joined: 8/12/2021 Last visit: 1/15/2026 Posts: 351 Rating:
|
Hi! Have you tried with a logic error in this outputs? Sometimes this states are usually overwritted. Maybe can helps you to define the state |
|
If this Information really helps, you could use the Rate function |
|
| 11/8/2024 8:15 AM | |
|
Posts: 15 Rating:
|
Logging the status of the PostPut block was one of the first things I did, It goes from 7000 to 7001, then 7002 (is all correct) and then to 8601. This means the TSEND_C block and I did a log of the TCON (inside of the TSEND_C bock) status and that one goes from 7001 to 7002 and then 80E1 The IT guys from the ERP system can't (or won't) help me much... So I have no idea if it is a problem with the certificate or some other problem... |
Follow us on