(0)| 5/23/2022 2:52 PM | |
|
Joined: 10/11/2006 Last visit: 1/8/2026 Posts: 6065 Rating:
|
Hello, the reference value for speed at the TO configuration doesn't suit to the referencevalue in the drive. Drive type: Analog drive connection Reference speed For a standard motor, the reference speed is the speed with which the drive rotates when 100% is output at the analog output. The reference speed must be configured for the drive and transferred in the configuration of the technology object. The analog value that is output at 100% depends on the type of the analog output. For example, for an analog output with +/- 10 V, the value 10 V is output at 100%. Analog outputs can be overridden by approximately 17%. This means that an analog output can be operated in the range from -117% to 117%, insofar as the drive permits this. Reference velocity With a linear motor, the reference velocity is the velocity at which the drive moves with an output of 100% at the analog output. The reference velocity must be configured for the drive and transferred to the configuration of the technology object. The analog value that is output at 100% depends on the type of the analog output. For example, for an analog output with +/- 10 V, the value 10 V is output at 100%. Analog outputs can be overridden by approximately 17%. This means that an analog output can be operated in the range from -117% to 117%, insofar as the drive permits this. 4.1.2.2 Configuration - Data exchange with the drive (S7-1500, S7-1500T) https://support.industry.siemens.com/cs/ww/en/view/109781849 |
|
With best regards, |
|
| 11/6/2024 9:28 AM | |
|
Joined: 3/9/2024 Last visit: 4/26/2025 Posts: 1 Rating:
|
问题不知道在哪? |
| 11/6/2024 10:08 AM | |
|
Joined: 3/30/2020 Last visit: 12/11/2025 Posts: 5656 Rating:
|
不要把注意力集中在当下,而要解释一下你想要达到的最终结果是什么? .. 在运动控制应用中使用DB_ANY数据类型的好处是什么? |
Last edited by: qwazee at: 11/06/2024 10:21:12Last edited by: qwazee at: 11/06/2024 10:21:53Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
|
|
| 11/12/2024 4:04 PM | |
|
Joined: 10/11/2006 Last visit: 1/8/2026 Posts: 6065 Rating:
|
Hello, Advantage of DB_ANY https://support.industry.siemens.com/cs/ww/en/view/109750880 SIMATIC S7-1500T: Using "REF_TO" and "DB_ANY" with technology objectshttps://support.industry.siemens.com/cs/ww/en/view/109822593 |
|
With best regards, |
|
Follow us on