(0)| 11/29/2024 5:25 PM | |
|
Joined: 4/22/2021 Last visit: 12/12/2025 Posts: 27 Rating:
|
Hi all. I need to collect data for further analysis, contained at DB, but only during commissioning / testing to fingerprint machine behaviour. Specifically I have 4 arrays of 256 LReal + some additional word / INT / Real / DTL data-points. All these data it is contained at one DB, and only need to be retrieved during engineering, not while machine it is in production, however we need to take many samples of it during machine tuning. Already observed some links suggesting:
Is there any option at TIA V19 engineering software that allows to do such a kind of thing smoothly, so exporting certain watchtable / DB or similar object containing required data, to a CSV file, or appending it to existing file or some kind of database file directly to engineering PC, not involving anything else than TIA engineering environment? Or best alternative it is only the link attached upwards? Thank you. |
Last edited by: Moderator_Lan at: 12/02/2024 09:50:11link optimized |
|
| 12/2/2024 3:31 PM | |
|
Joined: 7/7/2010 Last visit: 1/16/2026 Posts: 16379 Rating:
|
Look for and try Snap7. There are sample applications which you can configure to retrieve an entire DB - provided GET is allowed on the PLC (preferably without a password - and can be removed after commissioning). NOTE: Snap7 works with unoptimized data.
|
|
science guy |
|
Follow us on