(1)| 12/9/2024 11:35 AM | |
|
Joined: 5/11/2022 Last visit: 5/4/2025 Posts: 73 Rating:
|
Hello every body I have a problem with TIA portal 19 is it possible to help me? 1. PLC : S7-1500 V2.9 : SN:6ES7 518-4AP00-0AB0 2. Touch Panel: TP 1200 . SN:6AV21240MC010AX0 I want to connect PLC 1500 to TP1200.I have made a connection (PN/IE) according to instructions but the connection was not established properly and the data was not transfer between PLC and HMI. I have Read below file for this aim and I have found out that I should configure the access level. https://support.industry.siemens.com/cs/ww/de/view/109973173 I followed the instruction to configure access level and define a roll but it was not possible. I can not find HMI access in function rights according to the picture. in my function rights there are just 3 option (1.OPC UA server access 2.user authentication of the opc... 3.manage certificates). I would be pleasure if you tell me if this instruction just have wrote for s7-1500 v3.1? how can I configure access level in my project with PLC (S7-1500 V2.9)? because of some reasons I can not upgrade the PLC firmware. how can I solve my problem? |
Last edited by: goudarzi91 at: 12/09/2024 11:37:49Last edited by: Moderator_Lan at: 12/09/2024 12:07:11link optimized Last edited by: goudarzi91 at: 12/09/2024 12:13:46Last edited by: goudarzi91 at: 12/09/2024 12:18:15 |
|
Follow us on