(2)| 1/21/2025 4:30 AM | |
|
Joined: 1/21/2025 Last visit: 1/21/2025 Posts: 1 Rating:
|
To simplify the process for your service engineer, consider allowing them to input 10 or 20 key data points and then use linear interpolation to generate the full array of 1,000 integers. This approach reduces manual data entry and ensures smooth transitions between specified points. Implementing Linear Interpolation in TIA Portal Siemens provides resources on performing linear interpolation within TIA Portal. For example, the article "Interpolating measured values with polygon and output of function values" details how to execute linear interpolation via measured values and output new function values based on this polygon. Alternative Approach If you're open to using external curve fitting tool allows you to input a limited set of data points and perform interpolation to generate a smooth curve. You can then export the interpolated data and import it into your TIA Portal project. |
Last edited by: Moderator_Lan at: 01/21/2025 08:04:59Link optimized / Link removed, doesn't comply with forum terms |
|
This contribution was helpful to
|
|
Follow us on